Hello,
Recently i bought some SparkFun nrf52840 mini and SparkFun LSM9DS1.
The problem is that, sometimes, the board nrf52840 seems to get stuck and don’t even do the setup function. The conditions are a bit random, somethimes i upload code and works fine, but when i upload it again, doesn’t work.
This scenario occour in the following code:
#include <Wire.h>
#include <SparkFunLSM9DS1.h>
LSM9DS1 imu;
#define LSM9DS1_M 0x1E // Would be 0x1C if SDO_M is LOW
#define LSM9DS1_AG 0x6B // Would be 0x6A if SDO_AG is LOW
#define DECLINATION -8.58
int i = 0;
// the setup function runs once when you press reset or power the board
void setup() {
// initialize digital pin LED_BUILTIN as an output.
Serial.begin(115200);
while(!Serial) delay(10);
pinMode(LED_BLUE, OUTPUT);
digitalToggle(LED_BLUE);
delay(200);
Serial.println("Ok");
digitalToggle(LED_BLUE);
delay(200);
Serial.println("That works");
imu.settings.device.commInterface = IMU_MODE_I2C;
imu.settings.device.mAddress = LSM9DS1_M;
imu.settings.device.agAddress = LSM9DS1_AG;
}
// the loop function runs over and over again forever
void loop() {
i++;
Serial.print(i);
Serial.print(" - ");
if(imu.accelAvailable()){
imu.readAccel();
Serial.println(imu.ax);
}
Serial.println();
digitalToggle(LED_BLUE); // turn the LED on (HIGH is the voltage level)
delay(200); // wait for a second
}
When it doesn’t work, i have cases tha only the “Ok” is displayed in the serial monitor or even cases that i don’t get nothing.
Maybe is a problem with the serial communication.
If someone have a glimpse in how to fiz that or why this is occouring, i whould like to hear.
Thanks.