Just received my order from sparkfun for the DEV-19426. Since I was in a hurry, it of course doesn’t seem to work as expected.
I apply the supplied cable (USB-C) and the board powers up as expected.
I connect a qwicc device (SparkFun VR IMU Breakout - BNO080 (Qwiic) and the Artemis does not power up the connected device.
The BNO088 is known to work and powers up through same cable from other sparkfun boards.
My other sparkfun boards are powering up the BNO080 board via qwiic. The code snippet that looks for i2c devices isn’t finding anything connected.
The long term goal is to connect the SparkFun GPS-RTK Board - NEO-M8P-2 (Qwiic) and do some logging/averaging of locations that I want to make sure are highly accurate in their location description.
Can someone shed some light on why this isn’t working — did I get a dud or have I made a mistake?