Hey,
what is the orientation of the SWD J-link ports?
Hey,
what is the orientation of the SWD J-link ports?
Pin 1 has the little white line next to it.
Thanks.
No problem! ![]()
Does anyone have a working setup / configuration for connecting over JTAG / SWD? Tried JLinkExe, but none of the AmbiqMicro devices work.
Hi @gauteh,
I have had Segger Ozone working with the Artemis - I was using it to investigate some strange behavior on OpenLog Artemis with v2 of Apollo3. Please see this link - the screenshots come from Ozone: https://github.com/sparkfun/Arduino_Apo … -860016907
I was using a J-Link with Segger’s 50-Mil 10-Pin Patch Adapter. I soldered a 2x5 0.05" header onto the OpenLog Artemis SWD port to make it easy to connect the ribbon cable. I’ve attached a photo of the jumper configuration.
The Processor was set to: AMA3B1KK-KBR
I hope this helps!
Best wishes,
Paul



Just for reference, here are the connections from the 20-way J-Link pins to the 10-way SWD pins:
J-Link - SWD
1 - 1 VTREF (3.3V)
7 - 2 SWDIO
9 - 4 SWCLK
13 - 6 SWO
15 - 10 RESET
4/6/8/10/12/14/16/18/20 - 9 GND
SWD pins 3 and 5 are also GND
Thanks a lot! I managed to start a debugger using JLinkGdbServerEXE and gdb-multiarch, so things are working. I haven’t managed to use pyocd, seems like there might not be support in openocd for the ambig apollo’s.