Hello,
I would like to verify a few things about the SparkFun RedBoard Qwiic :
-
You cut the jumper to 5V and solder a blob to 3.3V and now the board runs at a 3.3V logic level?
-
Once setup for 3.3V, I can still use a 12V wall wart to power the device?
-
At 3.3V does the board still run at 16MHz or it is running slower (I see other 3.3V boards running at 8MHz)?
Thanks
- That is correct as mentioned in the [[hookup guide](https://learn.sparkfun.com/tutorials/redboard-qwiic-hookup-guide#hardware-overview) (click the **Jumpers** button), that jumper controls the voltage to the VCC pin of the ATmega328.
Just be aware if you are using a shield that uses the I/O Ref pin, that it is still tied to 5V. It was accidentally carried over from the previous design of the original RedBoard instead of being tied to that jumper selection.
- That is also correct, as shown in the [[schematic](https://cdn.sparkfun.com/assets/c/5/7/e/f/RedBoard-Qwiic.pdf) the 3.3V regulator (AP2112) takes 5V from the 5V regulator (LM117). As mentioned in the [[hookup guide](https://learn.sparkfun.com/tutorials/redboard-qwiic-hookup-guide#hardware-overview) (click the **Power/Reset** button), the LM117 can take 12 volts.
- I am pretty sure that crystals run at their resonant frequency once powered, so it should still run at 16MHz.](https://learn.sparkfun.com/tutorials/redboard-qwiic-hookup-guide#hardware-overview)](https://cdn.sparkfun.com/assets/c/5/7/e/f/RedBoard-Qwiic.pdf)](https://learn.sparkfun.com/tutorials/redboard-qwiic-hookup-guide#hardware-overview)
Thanks for the quick reply…that gives me the info I need.