Hello!
I am trying to program a SparkFun Thing Plus - STM32 board to write to an SD card using the integrated SD card breakout.
However, I keep encountering the FR_NOT_READY error when attempting to mount the card using the FATFS middleware.
Setup Details:
IDE/Tools: STM32CubeIDE with FATFS middleware and SDIO configured in a 4-bit wide bus.
Voltage: The SD card breakout is powered by 3.3V, which should be sufficient for my SD card (onn. 64GB Class 10 U3 MicroSDXC).
Detect Pin: From my understanding, this package does not have a Detect_SDIO pin.
Current Initialization Code:
int init_sd_card(void) {
res = f_mount(&fs, SDPath, 1);
if (res != FR_OK) {
printf(“SD card mount failed with error: %d\n”, res);
return 0;
}
printf(“SD card mounted successfully.\n”);
return 1;
}
Observations:
Debugging with a SEGGER J-Link shows the following values for SDPath (decimal representation):
[0] = 48, [1] = 58, [2] = 57, [3] = 0
The issue seems to originate in disk_initialize (inside diskio.c), which returns 1. This propagates to ff.c, causing the FR_NOT_READY error.
If I set the SDIO up as being 1-bit wide, then I make it further in the chain, where stat will be RES_OK, and the init function fails because of the error FR_DISK_ERR
Questions:
- Could the lack of a
Detect_SDIOpin be causing this issue? If so, what workarounds are recommended? - Could this be related to power or timing issues on the SDIO lines?
- Are there any additional debug steps or configurations I should check to identify the problem?
- Any solutions or experience?
Any advice or insights would be greatly appreciated. Thank you!
EDIT: When I run it in 1-bit wide SD, it will fully work when the clock is scaled down sufficiently. 8MHz is too fast, with a prescaler of 9 (1.45MHz) it works, 8 though is too fast