Spectral Triad (AS7265x) not responding.

Hallo,

I bought a sensor on your website and connected it according to the instructions.

I also passed the arduino nano and installed up-to-date libraries and examples, but arduino does not want to connect to AS7265.

the jumpers on the back and front sides are open.

I also tried to check it via uart, but it also does not respond to commands (I closed the jumper)

Please help to solve the problem.

i attached some images connections.

PastedGraphic-1.png


Thanks.

The blue and yellow wires go to SDA and SCL (it looks like they are mis-wired currently)…also if you are using i2c remove the solder from JP2 https://learn.sparkfun.com/tutorials/sp … okup-guide

If it still not doesn’t show up on i2cDetect you can cut the traces for the i2c pull-up resistors (there’s already a lot of resistance in the setup because of the multiple wire junctions)

HI,

i tried to cut the traces for the i2c but it not helped me.(checked with tester they are l2c open jp2 open too)

i tried 3 different arduino and got a same problem.

AS7265x Spectral Triad Example

Point the Triad away and press a key to begin with illumination…

Sensor does not appear to be connected. Please check wiring. Freezing…

One of the chips on this board is a 3.3 volt chip and it looks like you’re powering it with 5 volts.

That might have fried the chip and that would cause the board to not work anymore. :frowning:

I used boards with a voltage of 3.3v just before connecting, I measured the voltage with a tester and there was 3.3v

YellowDog:
One of the chips on this board is a 3.3 volt chip and it looks like you’re powering it with 5 volts.

That might have fried the chip and that would cause the board to not work anymore. :frowning:

I used boards with a voltage of 3.3v just before connecting, I measured the voltage with a tester and there was 3.3v

I have also had issues. I started with the qwiic connectors, and that didn’t work. I was using Nate’s library, and tried multiple codes. The code would hit the lines that checked if the sensor was active, and freeze:

if (sensor.begin() == false)

{

Serial.println(“Sensor does not appear to be connected. Please check wiring. Freezing…”);

while (1);

}

I then commented out the while(); (and added a small delay) just to force it to move on and show me what data it would take. I would then get zeroes for the data approx. 10 out of 11 times. But that one time, it would work (example below). I could move my hand across the sensor and it responded; it also would respond to various colors of light from my phone (i.e. the appropriate values would increase or decrease). Once it did work, it would continue working; the values would not spontaneously return to zeroes.

This <10% working-time happened with both re-uploading as well as simply hitting the UNO reset button. I then soldering in headers and tried the I2C there, and got the same result. I have only used 3.3V, never 5V. I have removed and reinstalled the library.

Any help would be appreciated.


AS7265x Spectral Triad Example

Sensor does not appear to be connected. Please check wiring. Freezing…

A,B,C,D,E,F,G,H,R,I,S,J,T,U,V,W,K,L

0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,

0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,

…

0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,

AS7265x Spectral Triad Example

Sensor does not appear to be connected. Please check wiring. Freezing…

A,B,C,D,E,F,G,H,R,I,S,J,T,U,V,W,K,L

0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,0.00,

…

AS7265x Spectral Triad Example

A,B,C,D,E,F,G,H,R,I,S,J,T,U,V,W,K,L

16.54,112.41,283.59,174.29,321.45,435.27,388.18,290.40,680.18,119.49,225.43,60.01,35.70,26.54,54.24,40.33,6.49,5.95,

16.54,112.41,283.59,174.29,321.45,435.98,388.18,290.40,680.18,119.49,225.43,60.01,35.70,26.54,54.24,39.24,6.49,5.95,

16.54,112.41,283.59,0.00,321.45,433.86,387.29,289.11,677.84,119.49,225.43,59.66,35.70,26.54,54.24,39.24,6.49,5.95,

15.71,112.41,283.59,0.00,322.19,435.98,389.52,291.26,684.86,119.49,225.43,60.01,35.70,26.54,54.24,40.33,6.49,5.95,

16.54,112.41,284.49,0.00,322.19,435.27,389.52,290.83,683.69,119.86,226.46,60.01,35.70,26.54,54.24,40.33,6.49,5.95,

16.54,112.41,283.59,174.29,322.19,435.27,389.07,290.40,683.69,119.86,225.43,60.01,35.70,26.54,54.24,40.33,6.49,5.95,

I found a workaround. In the void setup(){…} I put in a loop that checked to see if the sensor was responding:

if (sensor.begin() == false){ delay(500); }

else{ break;}

It would respond after anywhere from one to 20+ inquiries. However, once it did respond, it worked fine in the main void loop(){…} of the code. I guess it just needed a little attention to feel needed, and then it was happy to do its work. :smiley:

We are also facing same issues as posted by " pointsplitter". We have also posted one blog “SPARKFUN TRIAD (AS7265X) CONNECTIVITY ISSUES”.

We have posted some images and a video link for reference.

https://drive.google.com/file/d/1IyoyvB … sp=sharing

Kindly share the information to resolve the issues.