STR-E912 ARM-USB-OCD driver error?

Hello,

I’m using evaluation kit from OLIMEX,STR-E912

http://www.olimex.com/dev/str-e912.html

which use mcu STR912FW44x and I also use ARM-USB-OCD as my jtag. The software CD that comes with this evaluation kits contains

  1. eclipse version 3.20

  2. yagarto-bu-2.17_gcc-4.1.1-c-c++_nl-1.14.0_gi-6.5.5.exe

  3. openocd-2006re115-setup-rc01.exe

  4. yagarto-ide-20061002-setup.exe

  5. IDEaliST.exe

  6. sarm.exe

  7. IDEaliST-update.exe

and main program OLIMEX-GCCFD-190207.exe that install all of require program and example source code (lpc2106 blink led) to develop cross platform.

I’ve run OLIMEX-GCCFD-190207.exe and when install finish. It tells me that I’ve to install driver for jtag for three times when I plug JTAG to my computer. But when I’ve conneted ARM-USB-OCD to my computer it’s only ask me to install driver for 2 times (channel A and channel B). So I think it’s nothing wrong and keep go on.

First I think,I’ve to modified exaple code and find library of str91x.h and edit some file to work with this evalution board then use eclipse to download code via external tool that have config for my mcu.

When I call external tool on eclipse it say

Info: openocd.c:82 main(): Open On-Chip Debugger (2006-10-12 18:00 CEST)

Error: ft2232.c:1033 ft2232_init(): unable to open ftdi device: 2

Error: ft2232.c:1048 ft2232_init(): ListDevices: 2

Error: ft2232.c:1050 ft2232_init(): 0: Dual RS232 A

Error: ft2232.c:1050 ft2232_init(): 1: Dual RS232 B

  1. Is this the right method to work with this board and JTAG?

NOTE : I’ve copy config file for openOCD from this webboard

  1. Is Jtag driver installation have a problem ?(2 times instead of 3)

  2. Could you please recommend me how to work with this evaluation board? Some example code that can run on this evaluation kits nad Jtag? (I want to test that my board and ARM-USB-OCD are working properly)

NOTE : I bought two evaluation board and test with the same process.The problem is the same.ToT

Thanks for all reply

Ukyo

Hello, I can’t help you out as I just received my board today.

I know absolutely nothing about it, yet, I hope.

But I have a follow-up question for you, if you don’t mind.

I never received any software for the board and it looks like you received some files that I would not mind having?

Some I am assuming I could find on the net, but some maybe not. Is there anything that would make sense to share with me?

Thanks,

Dustin

Hello Ukyo,

perhaps you should ask Olimex if they can help you?

But you can take a look at the following page too:

http://openfacts.berlios.de/index-en.ph … CD_scripts

Here you will find a STR912 setting for the OpenOCD, take a look at it.

The OpenOCD from YAGARTO setup has no config file for the STR912

because I have no STR912 board for testing.

@Olimex,

It looks that you now put YAGARTO on your CD? It would be nice to

got only a short note if you do that.

Best regards,

Michael