Hi,
does anyone have complete script for flashing/debugging str9 via arm-usb-ocd?
Reg
Hi,
does anyone have complete script for flashing/debugging str9 via arm-usb-ocd?
Reg
Use my str9 script here:
http://www.sparkfun.com/cgi-bin/phpbb/v … php?t=4812
just changing the interface and jtag speed:
interface ft2232
ft2232_device_desc “Olimex OpenOCD JTAG A”
ft2232_layout olimex-jtag
jtag_speed 1
…
Regards
Spen
thanks ntfreak!
for all newbies like me
here is config file which works with STR-E912 board and ARM-USB-OCD!
note: don’t forget to remove jumper RST-TRST from STR-E912 board!
if you have other board check for trst and srst signals on your board and your reset_config parameter!
file arm-usb-ocd_str9.cfg (thanks to ntfreak):
##debug 3
telnet_port 4000
gdb_port 2000
interface ft2232
ft2232_device_desc “Olimex OpenOCD JTAG A”
ft2232_layout olimex-jtag
jtag_speed 1
# !!!For Olimex STR-E912 board you must remove jumper RST-TRST!!!
reset_config trst_and_srst
jtag_device 8 0x1 0x1 0xfe
jtag_device 4 0x1 0xf 0xe
jtag_device 5 0x1 0x1 0x1e
##target arm966e little run_and_halt 1 arm966e
target arm966e little reset_halt 1 arm966e
daemon_startup reset
##run_and_halt_time 0 0
working_area 0 0x50000000 16384 nobackup
flash bank str9x 0x00000000 0x00080000 0 0 0
first run deamon with this config file:
openocd-ftd2xx –f arm-usb-ocd_str9.cfg
then it is possible to for example flash STR9 device via telnet at port 4000:
telnet localhost 4000
commands for flashing (for details look at http://openfacts.berlios.de/index-en.ph … D_commands or at http://www.fh-augsburg.de/~hhoegl/proj/ … ickref.pdf):
str9x flash_config 4 2 0 0x80000
flash protect 0 0 11 off
flash erase 0 0 2
flash write 0 lcddemo.bin 0x0
Hi,
I have done everything that has been mentioned in this thread but I am
unable to get this setup completely working. My openocd can validate the
JTAG chain and starts up nicely. I can connect using telnet and get help and
do only CPU specific commands. For all the other commands like dumping
memory or when i try to program the flash it gives me an error saying
the target must be halted before this operation can be performed.
When I try to halt the target it just times out
I have tried to use the
multi-ICE+ AXD 1.2 combination with an In Circuit Emulator also but the
same thing happens. Multi-ICE is able to validate the JTAG chain and is
able to see the three devices but AXD 1.2 fails to halt the target.
Can somebody please help me with this.
tomhawk
PS: I have already removed the TRST_RST jumper.
Hi,
could you please tell us a bit more about your target board, your JTAG interface and the version of OpenOCD you’re using?
You should always use the latest OpenOCD version available, either compiled yourself from SVN or using the binaries provided by www.yagarto.de.
Regards,
Dominic
Hi Dominic,
Thanks for the reply.
The target board is Olimex STR-E912 that has a STR912(ARM966) on board.
I got a package on a cd from olimex when I bought the Olimex
ARM-USB-OCD from them. It installed openocd version r115, the FTDI driver and eclipse on my machine. I assumed this configuration would work as
everything was coming in a package from them.
I can try the new version of openocd. I will let you know if that works.
Thanks,
tomhawk
Hi,
if it doesn’t work send me a log file (run with -d -l ) to Dominic Rath gmx de.
Regards,
Dominic
Hi Tom,
a few things for you to try:
increase the jtag_speed divisor (try 10, and if it works, reduce it gradually)
change daemon_startup to “attach” instead of “reset”
change “reset_halt” in the target line to “run_and_halt”
It would be best if you could try each change individually.
Regards,
Dominic
Hi Tom,
I tried each of them individually but none of them worked.
Thanks,
Tom
Hi Tom,
could you try reading the “comms_ctrl” register:
(at the telnet prompt, with “daemon_startup” set to “attach”)
reg comms_ctrl
and paste the result.
Regards,
Dominic
The comms_ctrl value is
reg comms_ctrl
comms_ctrl (/32): 0x60000000
Thanks,
Tom Hawk
That value is ok, the mystery deepens.
A log file would be the next step.
Spen
Hello Spen,
I’ve forwarded you the log that Tom sent me yesterday.
Regards,
Dominic
Hi Tom,
as Spen already said the comms_ctrl value of 0x6… (denoting EmbeddedICE Rev6) is fine - I thought/hoped that maybe there were different revisions of the STR9x using different ARM9E-S cores, but apparently your chip is exactly the same as Spen’s.
Is there already code running on your board?
If there is code, is that code working at the time you’re trying to halt it?
You could try a very slow JTAG frequency, like “jtag_speed 100”.
Regards,
Dominic
Hi guys,
I got it somewhat working with some error messages but the code is
running fine and I am able to halt the target. Here is what I did.
I changed the jtag reset to
“reset_config trst_only”
Also, I put the “trst_rst” jumper back on. here is the output of the
openocd when I used that configuration.
Info: openocd.c:84 main(): Open On-Chip Debugger (2006-01-26 13:30 CET)
Error: jtag.c:832 jtag_add_reset(): requested nSRST assertion, but the current configuration doesn
't support this
Warning: arm966e.c:105 arm966e_assert_reset(): can’t assert srst
Warning: arm7_9_common.c:848 arm7_9_halt(): target was in unknown state when halt was requested
Warning: arm7_9_common.c:623 arm7_9_poll(): DBGACK set while target was in unknown state. Reset or initialize target before resuming
regards,
tomhawk