First of all, I can’t find a Vista driver for this device, which is a problem. However, since UsbDeview can display the device, I was hoping I’d be able to operate the board via OpenOCD. I’m already using OpenOCD to access an Olimex ARM-USB-OCD, which uses the same FTDI FT2232 as this board does. However, in spite of several attempts with different cfg files, I haven’t been able to connect to the device; I always get “unable to open ftdi device: 2”. (Device 1 is the Olimex, Device 2 is the ComStick).
Is this just because I don’t have a Vista driver installed, or is it because my config file is somehow wrong? I can post my file here, but I thought I’d wait until I know there’s a reason to do so.
In the meantime, is there a Vista driver for this device somewhere? A web search didn’t turn up anything.