Hi I want to erase the flash of an STR9. I’m using Amontec JtagKey and Openocd rev278 but I got this problem:
Info: openocd.c:93 main(): Open On-Chip Debugger 1.0 (2009-03-06-16:03) svn:278
Info: openocd.c:94 main(): $URL: http://svn.berlios.de/svnroot/repos/openocd/trunk/src/openocd.c $
Error: ft2232.c:241 ft2232_read(): couldn't read the requested number of bytes from FT2232 device (0 < 81)
Error: ft2232.c:385 ft2232_send_and_recv(): couldn't read from FT2232
This is my cfg file
#daemon configuration
telnet_port 4444
gdb_port 3333
#interface
interface ft2232
ft2232_device_desc "Amontec JTAGkey A"
ft2232_layout jtagkey
ft2232_vid_pid 0x0403 0xcff8
jtag_speed 6
jtag_nsrst_delay 200
jtag_ntrst_delay 200
#use combined on interfaces or targets that can't set TRST/SRST separately
reset_config trst_and_srst
#jtag scan chain
#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
jtag_device 8 0x1 0x1 0xfe
jtag_device 4 0x1 0xf 0xe
jtag_device 5 0x1 0x1 0x1e
#target configuration
daemon_startup reset
#target <type> <startup mode>
#target arm966e <endianness> <reset mode> <chainpos> <variant>
target arm966e little reset_init 1 arm966e
run_and_halt_time 0 30
working_area 0 0x50000000 16384 nobackup
#flash bank <driver> <base> <size> <chip_width> <bus_width>
flash bank str9x 0x00000000 0x00080000 0 0 0
#Script used for FLASH erasing
target_script 0 reset /home/ale/str9_cfg_openocd/str91x_flasherase.ocd
And this is the ocd file
wait_halt
str9x flash_config 4 2 0 0x80000
flash protect 0 0 10 off
flash erase 0 0 10
reset
shutdown
Anyone can help me?
Thanks!