I’ve been stuggling with lagging timestamp on the Datalogger-IoT-9dof device, and hence connected a RTC RV-8803 using the qwiic connector. To test the RTC, I disabled the WiFi and changed the time setup settings to use the RV8803 as the reference clock and the logger settings should return a datetime. This is the date return value:
23-08-2024 00:36:40,08/22/2024,22/08/2024,22:36:40,2024-08-22T22:36:40,2024-08-22T22:36:40+00:00,Thursday,Thu,22nd,August,Aug,2024,1724366200,
How can set the return value to a dd/mm/yyyy-HH:MM:SS format ?
You should be able to adjust the setting for USA/other in the menu here