i currently have acsess to two prettty awesome devices one of the older 80 GB Zunes and an [Ematic MP3
So the screen on this Mp3 is broken while the Zune completely wipes its memory after downloads.
The Mp3 has a integrated mic and camera ( that works as a webcam by going to settings and then clicking on webcam and plugging the mp3 into the pc) so yeah this little thing has some amazing features. As for the zune it has like 20 times the GB (maybe even more) of that mp3 so that would be nice to have.
How Would I Get the MP3 be able to be viewed on the zune screen using wiring + other methods? that is the main goal i have but my secondary is being able to use that 80gb from the zune one way or another. This is not neccesary, but i would like still be able to play music and all that on the zune player. Also if no one thinks this is possible or gets what i am saying if you could help me just fix the zune and how it wipes itself that would help too :D](http://www.ematic.us/product_details.php?prodID=84)