Seems like it would be simpler and less costly if the Arduino can access the Internet via wired cat5 or WiFi. Then it can send SMS to a dumb phone or SMS/email to a any smart phone. This presumes the Arduino system is not on wheels.victorf:
I would like to be able to build an Arduino based system that has the ability to send textual data (via SMS?) to a 'Droid cell phone. The system gathers data from several sensors, computes the results from the data and formats the results in standard text packets (i.e. “hhhhh, ddd, sss, ”). Individual packets would never exceed 30 bytes. The data would need to be sent every 15 or 30 seconds for approximately 10 minutes. Might it be possible to send the all the data in a burst of packets by accumulating them until the end of collection then sending them all?Is such an application feasible from the communications viewpoint? What sort of hardware would I need to look at for the communications aspects?
Any enlightenment will be appreciated.
Vic