I am working in Eagle and want to use the Teensy 4.0 with USB Host capabilities.
My plan is to use the Teensy 4.0 footprint from the library at GitHub - eagleman1022/Eagle-Library-Teensy: This repository holds the Eagle Cad library for the Teensy 3.6 and newer. There may be more than one version of each device to better facilitate varying usage. · GitHub and delete the pins I am not using (leaving only the 14 pins on each side and the pins for USB Host D+ and D-).
Here are my questions:
-
Can someone confirm that the D+ and D- pins in the footprint in Eagleman’s library file are placed appropriately for pogo pin connection to the D+ and D- pads on the Teensy 4.0?
-
Is the spacing between the D+ and D- pads 1.8 mm?
-
Is the location and dimensions of the D+ and D- pads documented anywhere on the PJRC or sparkfun pages?
-
Can anyone identify the pogo pins this footprint was designed for? The drill seems just a little small for the Mill Max pogos I looked at.
Thanks for any help anyone can provide.