Check your signal level (AT+CSQ?). If you don’t have a good signal you won’t connect. If the signal level is OK, check the registration state (AT+CREG?). This will tell you if the radio is searching for a cell, or if registration has been denied.
I would like to know if there are some commands that allows the modem to notify to the rs-232 interface the arriving of an SMS from the network without need of extra software/hardware to poll the AT commands?
I need the module to notify directly to the RS-232 port the arrival of new SMS automaticaly. How do I set the modem to do that?
Look at the “AT+CNMI” command. This allows you to set various options for the radio send you unsolicitied commands (AT+CMTI) when messages are received.
nejemiagrodzicki:
I have now the GM-862 module working fine.
I would like to know if there are some commands that allows the modem to notify to the rs-232 interface the arriving of an SMS from the network without need of extra software/hardware to poll the AT commands?
I need the module to notify directly to the RS-232 port the arrival of new SMS automaticaly. How do I set the modem to do that?
Thanks a million.
Hello I have the same problem you asked first. How did you fix it?
I seek in the CREG and all it says is 0.3 and 0.2. Making a Network survey this returns that all my networks are Forbidden.
I have bought a telit GM862 module with easy GSM/GPRS Board, and I connected everything, but when I turn the power ON, the status LED keeps blinking for 7 times then turn off and the module still turned off, although I made sure of the power supply that its 3A current and 3.8v,I dunno what to do to more to turn it ON??