My first post here, guess it’s sorta an introduction, kinda…
This is really my first attempt at designing, modeling, and implementing a functioning low voltage circuit. I say low, to me anything under 120v is low voltage…
The problem… My A/V receiver runs hot and I want to cool off it’s innards.
Solution…ish… So I wanted to run two separate computer case fans running on two separate temperature sensors, essentially a HIGH and LOW temp fans, I decided to make it fancy and add different color LED’s so I would know when what is running. I found myself in a conundrum of sorts as all of my knowledge is on mechanical jobs; I can TIG weld you a trailer, rebuild your car motor, and frame/plump/wire/drywall an extension to your house. Well all of that gets me nowhere in this current project.
So I wandered through some electrical engineering articles, brushed up on the components and their uses, watched a few basics on youtube and eventually found myself at [Everycircuit and what a neat little site that is. Amazon has since furnished my tinkering needs as far as components go, that and Fry’s Electronics.
So if you’ve made it this far I thank you and commend you, trying not to be too long winded but also what to convey that I don’t want the easy answer. I want to learn how to do this properly.
Here is an image of what I have so far… In the circuit I’ve replaced the switches with 10K ohm thermistors and the lights with 12v 80mm case fans
http://i1083.photobucket.com/albums/j39 … as39gc.pngAnd every thing works, kinda… With a 10k trim pot I get 4v to the fans, enough to turn them on but not enough to move any real quantity of air. So I try a 1K trimp pot, now I’m getting 1.5v to the fans… weird… so I put a 500k trim pot and I get 5.5v to the fan… Now we’re talking. I don’t get it though.
What am I witnessing here?? Because it’s going AGAINST what I thought should happen. AND it’s not what is predicted by the computer application which says I should be seeing 10.2v at the “fans”, HOWEVER the schematic doesn’t account for the thermistors…
Do I need lower resistance thermistors? On top of all this I’m still trying to figure out how to determine which transistors are best for this application.
Feed a man for a day, or teach him… I’d rather be taught. Thank you for your patience.
Nick](http://www.everycircuit.com)