the S3C44B0, s3c2410 support

Hi :

S3C44B0, S3C2410 are fully supported by openocd, if not, where can download relative configuration.

thanks!

why, no voice

The OpenOCD doesn’t support individual microcontrollers, but the ARM cores used in these uCs. Currently, the OpenOCD includes support for

  • arm7tdmi(-s)

  • arm720t

  • arm920t

  • arm922t

  • arm960e-s

If these Samsung(?) chips use one of the above cores, they’re supported. See http://openfacts.berlios.de/index-en.ph … figuration for a documentation of the config file options available.

Regards,

Dominic

Hi qchen10,

Your both mpu are supported by OpenOCD JTAG server:

SAMSUNG S3C44B0 > ARM7TDMI

SAMSUNG S3C2410 > ARM920T

Best regards,

Laurent

http://www.amontec.com

Hi:

I start the openocd with arm7_wig_cfg(at openocd\doc\configs) on my samsun S3C44B0 (arm7tdmk core) board with wiggler jtager . found warning message (please refer to attachment) and the system as if hang up, can’t input from the keyboard. i believe should be arm7_wig_cfg isn’t match the S3C44B0, but i don’t know how to modify this.

could you help to provide some information to solve it.

the attatchement as if can’t send,the warning as below:

info: openocd.c:82 main(): open on-chip debugger <2006-09-28 20:00 CEST>

Warning: arm7_9_common.c: 679 arm7_9_assert_reset(): srst resets test

logic, too

thanks

This warning is normal.

Now you should try, from another terminal, to connect to openocd using

telnet localhost 4444

or by attaching from gdb with

" target romote localhost:3333"

regards,

Magnus

it’s very good, thanks magnus

Best Regard