problem of code… I want to write to serial port every elapsed 10 seconds and every elapsed 20 seconds and every elapsed 30 seconds. My code is writing only one time 10 , 20, 30 elapsed seconds. Which code I must add ?? these 3 thread must be work standalone, there must be a way for this ? ![]()
const int ledPin = 13; // the number of the LED pin
// Variables will change:
int ledState = LOW; // ledState used to set the LED
long previousMillis = 0; // will store last time LED was updated
// the follow variables is a long because the time, measured in miliseconds,
// will quickly become a bigger number than can be stored in an int.
long interval = 999; // interval at which to blink (milliseconds)
void setup() {
// set the digital pin as output:
pinMode(ledPin, OUTPUT);
Serial.begin(9600);
}
void loop()
{
// here is where you’d put code that needs to be running all the time.
// check to see if it’s time to blink the LED; that is, if the
// difference between the current time and last time you blinked
// the LED is bigger than the interval at which you want to
// blink the LED.
unsigned long currentMillis = millis();
if(currentMillis - previousMillis > interval) {
// save the last time you blinked the LED
previousMillis = currentMillis;
// if the LED is off turn it on and vice-versa:
if (ledState == LOW)
ledState = HIGH;
else
ledState = LOW;
// set the LED with the ledState of the variable:
digitalWrite(ledPin, ledState);
if (currentMillis == 10000)
{
Serial.println(“10 seconds elapsed”);
}
else if (currentMillis == 20000)
{
Serial.println(“20 seconds elapsed”);
}
else if (currentMillis == 30000)
{
Serial.print(“30 seconds elapsed”);
}
}
}