TinyIR™ Learning IR Remote Control Receiver firmware

If someone could help me, to get firmware for this devise.

http://www.tauntek.com/tinyir-learning- … ceiver.htm

There ware all what we need for assemble receiver exclude firmware.

Or for that analog device like that one

http://www.tauntek.com/tinyir2-learning … ceiver.htm :roll:

send email to

rlgrieb@att.net

and ask for the .hex or source code. You may wish to explain your need and what hardware target you have in mind, if that hardware is not that which is sold by tauntek.com.

Ask for .hex code. I already assemble hardware which is sold by tauntek.com and need code.

http://www.tauntek.com/TinyIR2-assembled-kit.jpg

Didn’t they give you the already programmed chip with the kit?

perhaps the OP has a clone, hence the difficulty.

brainwav:
Didn’t they give you the already programmed chip with the kit?

I didn’t buy the kit on tauntek.com, I assembled it myself.

Did you email them and ask for the code? There’s also a free arduino lib that does all this and more, of course you’d have to port it to PIC. I’m about to do this for a project, but making it a greatly simplified version.

http://www.arcfn.com/2009/08/multi-prot … brary.html

Me.

Hello,

Did you use the libraries to make something similar as below?

http://www.tauntek.com/irmimic-learning … mitter.htm

It should be single chip solution for IR learning and transmitting.

Their chip costs 10 USD which is way too much. I want similar chip but for max. 2-3 USD.

So I don’t need the actual key pad, just an MCU interface to integrate in an electronic circuit.

The chip should operate in 2 modes: learn mode and playback mode.

The chip should be able to learn, and play back the stored IR pattern on demand.

Minimal 16 IR commands should be storable.

Regards,

/Pascal