Trace width

I am trying to use the trace width calculator from 4pcb. I am also ordering the $33 board from them. From their specs sheet I see 0.062", 1 oz. cu. plate. Does 0.062" correlate to the thickness on the calculator in mils? Thanks in advance.

Diego

http://www.4pcb.com/trace-width-calculator.html

http://www.4pcb.com/33-each-pcbs/

0.062" is the board thickness!

Ahhhhh. Thanks. So is the thickness 1oz/ft^2? The spec sheet only says 1oz cu.?

Yes. 1 oz copper is 1.4 mils.