Track thickness into 0603 resistor pads?

hello

is it ok to route 0.5mm tracks into 0603 resistor pads.?

Do you know what is the maximum track thickness that can be routed into 0603 resistor pads?

I am wondering if 0.5mm tracks will extract too much of the surface mount soldering heat out of the 0603 pads during the soldering process.?

A 0.5mm trace is ~20mils. An 0603 SMD is 30mils wide and I do use 20mil traces without issues.

Yes, it’s fine, and you can use a track that’s as thick as the pad if you like.

Assuming you’re mass producing the board, your CEM should profile it before committing to a large run. This process involves analysing the board layout and choosing a reflow profile accordingly. Normally it’s large components like big ICs which end up as the cold spots that need some extra heat.

If you’re soldering by hand then it’s a non-issue, just hold the soldering iron on the component a little longer until the solder starts to flow properly. You may possibly find components are a bit more difficult to remove should you need to - in which case two soldering irons are better than one!