trouble with AVR-PG2B

I got my AVR-PG2B parallel programmer and AVR-P20B-10MHZ development board today.

I’ve been trying to program an AT90S1200 chip with a hex file with AVRDUDE. Jumper J1 is open.

Below is the output from avrdude, it fails every time, however it does seem to detect the 1200 chip(0x1e9001).

I’ve tryed changing the settings on the parallel port (EPP or ECP) and i’ve tryed using a different computer ( though that perhaps i blew the port).

Any suggestions to what i’m doing wrong?

-=-=-

C:\blink>avrdude -p 1200 -c stk200 -P lpt1 -U flash:w:“blink.hex”:a

avrdude: AVR device initialized and ready to accept instructions

Reading | ################################################## | 100% 0.00s

avrdude: Device signature = 0x1e9001

avrdude: NOTE: FLASH memory has been specified, an erase cycle will be performed

To disable this feature, specify the -D option.

avrdude: erasing chip

avrdude: reading input file “blink.hex”

avrdude: input file blink.hex auto detected as Intel Hex

avrdude: writing flash (16 bytes):

Writing | ### | 6% 0.00s ***failed;

Writing | ######### | 18% 0.09s ***failed;

Writing | ################ | 31% 0.19s ***failed;

Writing | ###################### | 43% 0.28s ***failed;

Writing | ############################ | 56% 0.38s ***failed;

Writing | ################################## | 68% 0.47s ***failed;

Writing | ######################################### | 81% 0.56s ***failed;

Writing | ############################################### | 93% 0.66s ***failed;

Writing | ################################################## | 100% 0.75s

avrdude: 16 bytes of flash written

avrdude: verifying flash memory against blink.hex:

avrdude: load data flash data from input file blink.hex:

avrdude: input file blink.hex auto detected as Intel Hex

avrdude: input file blink.hex contains 16 bytes

avrdude: reading on-chip flash data:

Reading | ################################################## | 100% 0.00s

avrdude: verifying …

avrdude: verification error, first mismatch at byte 0x0001

0xc0 != 0x00

avrdude: verification error; content mismatch

avrdude: safemode: Fuses OK

avrdude done. Thank you.