Trouble with help system in uVision and Keil EPM900 emulator

I have just purchased the Keil EPM900 Emulator/Programmer, and after installing the uVision software (many times), I am unable to use the help system via the help button at the top of the screen. A message box which pops up says that the help files could not be found. Keil’s support suggested that I update the software from version 3V3.22a, to 3V3.30c. I have done so but the problem still exists. Can someone please tell me what files should be present in the UV3 folder within the uVision software? My theory is that the help files are not present after my installation. I am using Windows XP and the Microcontroller of interest is the Philips LPC936. I can write code and perform emulation with this software and hardware, so everything else looks OK.

Thanks.