Troubleshooting the WiFly shield for Arduino

Hello!

I’m having a tricky problem with the WiFly Library. The WiFly are connecting beautifully at home (airport express, WPA2) but not at my studio (WPA mixed). It doesn’t error out or associate, it just sits on the begin() call. I tested it out with the SpiUartTerminal sketch, and it looked good. I got this:

<2.21> set wlan ssid Method

AOK

<2.21> set wlan phrase xxxxxxxx

AOK

<2.21> set wlan auth 4

AOK

<2.21> scan

<2.21>

SCAN:Found 7

Num SSID Ch RSSI Sec MAC Address Suites

1 SmartFi 01 -67 WPAv1 74:91:1a:0f:7e:a9 AESM-TKIP 3104 0

2 MuseGames 02 -69 WPA_Mix 00:24:01:6f:8a:bd AES/TKIPM-TKIP 3104 0

3 shadygoliath1 06 -73 WEP 00:26:62:0d:1a:f6 1104 2

4 M3 Entertainment 09 -69 WPA_Mix 0c:d5:02:1e:42:b5 TKIPM-TKIP 1104 6

5 Method 11 -55 WPA_Mix 00:26:b0:fe:8b:a3 AES/TKIPM-TKIP 3100 0

6 DHAwifi 11 -62 WPAv1 00:21:29:ae:62:8e TKIPM-TKIP 1104 0

7 DHAguest 11 -74 WEP 00:15:e9:1e:d2:f8 3104 0

join # 5

DeAuth

Auto-Assoc Method chan=11 mode=MIXED SCAN OK

Joining Method now…

<2.21> Associated!

DHCP: Start

Method’s ssid is showing up at WPA mixed - so it seems like all should be good. Any thoughts? I’m super stuck and really want to get this working at this location. Thanks so much in advance!

Claudia