Hi Everyone,
Does anyone know where I can find the drivers for Telit UC864 to communicate with my PC? I have a EVK2 development board connected to the Telit UC864 interface board and when Im trying download the drivers for the USB, but it is unable to find the drivers online. And it didn’t come with a CD 
Could anybody answer my Q ?
Thanks in advance.
3G Terminal with RS232 and USB (UC864, HC25/HC28/HC15 etc.)
[1]. OS support
[2]. How to make connection with broadband ISP
[3]. How the terminal will transmit and receive the data over broadband.
when it is connected to PC/Embedded board via USB. Which USB class it uses
for Tx/Rx.
[4]. How PC/embedded board will communicate to 3G modem while operating a
call control, when it is connected via USB.
[5]. What are those sample reference applications will get in package.
[6]. As it support GSM/GPRS and CDMA, how it differentiates among these.