Upgrade to … ARM9 series …
ARM 926 et al are more complicated for memory protection .
and split instructions and Mem Fetches .
ARM 7 has a simple OP Code / Data fetch , only one path .
yet still addresses lots of External SRAM.
For the battery power consumed , a ARM 7 will run as fast
as a ARM 9 .
STR 710FZ2 T6 has 144 pins . and 65KB SRAM and 256KB Flash .
It will run as fast as any ARM 9 , power for power .
The problem is ppl load up a bad O.S. , then try to sell
the public on another mcu ! Its merely dirty competition !
The world got improved mcu’s , after T.I. got some German
to write the instructions for the TMS430 . But soon ARM was selling
so well , the 430 took a dive .
ARM 7 has reduced instruction set , and , REG to same REG ,
shift and add “multiply” . One clk multiplies and loads result
back into same register . w/o moving the register thru a long path .
With good 16Kb O.S. , STR710FZ2 can outrun all competition .
My project is battery powered ARM 7 , with a fast and a slower
path to slave ARM 7 's ( HC574 parallel , SPI serial paths ) .
Slaves NEVER talk fast to the main 7 , but main 7 must dnload
fast to slaves , cause slaves cant store , on their own mass-sto-device .
Slaves must be able to change context , quickly . Its the main7 , that
communicates with a human , then sends slaves , the new task .
Each slave can have a BG Micro $10 LCD 64-128 , to display
the analog voltages that it reads from its sensors . Slaves use plenty
of HC595 and SPI , to control hardware .
ARM 7 STR710FZ2 T6 is the fastest , and lowest cost …
$8 …