At first I tried installing this on Linux, but could not get it to open in PulseView. After hours of troubleshooting, confirming driver locations and udev rules, I eventually gave up and switched to my Windows 10 laptop. Windows is generally easier to get hardware/drivers working, but unfortunately I’m not having any better luck there. I’ll continue the below troubleshooting form Windows, but can switch back to Linux any time if it helps.
After going through your instructions provided ([Using the USB Logic Analyzer with sigrok PulseView), plugging in the device and installing the Zadig drivers, going to Pulse View and connect to Device, fx2lagw (generic…), USB, scan, I hear Windows indicate a USB disconnect/reconnect and the Device shows up in the box “Saleae Logic with 8 channels”.
However, from here, no combination of reinstalling Zadig drivers or simply selecting Ok seem to work.
(Reference screenshot in following post): Detailed PV log shows the firmware file found, uploaded 4096 bytes, then uploaded 4024 bytes, a few more lines, then “Device failed to renumerate”. At this point Device manager shows the Unknown Device #1 with status “this Device cannot start, an invalid parameter was passed to a service or function”.
I’ve been all through the troubleshooting steps provided, these forums, and several google searches, but cannot get past this point. It really seems like a hardware issue to me, but I’m happy to continue troubleshooting if you have any suggestions.
Thanks,
Jesse](Using the USB Logic Analyzer with sigrok PulseView - SparkFun Learn)](USB Logic Analyzer - 24MHz/8-Channel - TOL-18627 - SparkFun Electronics)