I like connect to phone for bluetooth using DUN profile of phone.
If i use PC, i can connect to phone using dongle bluetooth at DUN COM port and interact it with AT commands to recive and send calls and sms
but if i try to use bluesmirf to connect to phone, i can detect it, but it seems that only connect using SPP and don’t respond to AT commands.
In BlueSmirf command mode, i change de mode tu master (SM,1), them i realize the inquiry (I,30), the phone is detected…
¿What is the next setp?
If i try SR,{btdir] and then C, it connect, but never reply AT commands, (not dun mode??)
If i try to change profile mode, S~,{0,1,2,34}, and then connect, the result it’s the same.
What is my fault?
Why i can’t connect to phone using bluetooth dun profile and interact as modem with phone?
Thanks in advance.