I am a bit confused with the basic setup/commands to use OpenOCD/GDB for debugging the AT91SAM7 series with an Olimex “wiggler”. It is working strangely from what I am used to. (I’ve had a little experience setting up j-link/jlinkgdbserver and GDB, but gave up because there is little support for jlinkGDBserver.)
I’d like to be able to
- 
Halt code running from flash 
- 
“Completely” reset processor 
- 
Run code from 0x0 
First thing: When I connect to OpenOCD with GDB (target remote localhost:3333), my target halts execution immediately. Why? When I was using the Jlink, I would have to specifically issue a “monitor reset” command. This isn’t serious, it’s just peculiar.
Second: On my SAM7X board, OpenOCD apparently can not do a full hardware reset. I see this because after execution halts, and I issue a “monitor reset halt” command, some of the LEDS on the PIO lines may still be lit up. Also, “monitor reset halt” does not set pc to zero. Shouldn’t it?
- Joe
Here is the config file I am using:
# openocd cfg file for AT91SAM7S/X
# For more information about the configuration files, take a look at:
# http://openfacts.berlios.de/index-en.phtml?title=Open+On-Chip+Debugger
#daemon configuration
telnet_port 4444
gdb_port 3333
# When daemon starts, you can "reset" target or simply "attach"
daemon_startup attach
#interface setup for wiggler
interface parport
parport_port 0x378
parport_cable wiggler
jtag_speed 0
#On AT91SAM7S64-EK ans AT91SAM7X256-EK, TRST is always pulled up.
reset_config srst_only
# Wait after reset in ms
# I just picked an arbitrary value to see if it makes any difference
# (it can't hurt, can it?)
jtag_nsrst_delay 100 
#jtag scan chain
#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
jtag_device 4 0x1 0xf 0xe
# The target is halted after gdb connection.  Why?
# I am assuming this startup mode is what defines what happens 
#target <type> <startup mode>
#target arm7tdmi <reset mode> <chainpos> <endianness> <variant>
#This works on SAM7S:
#target arm7tdmi little run_and_halt 0 arm7tdmi_r4
#run_and_halt_time 0 30
#Try this:
target arm7tdmi little reset_halt 0 arm7tdmi_r4
###### Flash stuff untested #######
# For AT91SAM7, flash config values are looked up after reading the chip-id and type
flash bank at91sam7 0 0 0 0 0