At the moment i am looking for some kind of implementation of the STL für arm microcontrollers. Currently i am Using Yagarto, which includes libstdc++.a but im not quite sure what really is within that library.
Is STL implemented? If yes, how to use it e.g. to work with a list?
If not, what would be the best way to build a working implementation. STL port?
looking forward to get some hints ^^
Thorsten F:
At the moment i am looking for some kind of implementation of the STL für arm microcontrollers. Currently i am Using Yagarto, which includes libstdc++.a but im not quite sure what really is within that library.
Is STL implemented?
GNU libstdc++ does contain an STL implementation (remember that the STL is a set of Templates, and requires the header files).
Be warned that the STL will lead to code bloat. I would strongly suggest playing around with -fwhole-program and -combine compilation flags.
#include <list>
int main()
{
std::list<int> a;
a.push_back(1);
}
Ok i found the corresponding headers (just forgot to add the include dir)
What do you mean with those compiler flags?
If i just instantiate an empty list, everything is ok and working. Code size about 5kb. a simple push_back() increases code size to ~64kb and nothing works anymore 
Anyone has an Idea?
edit: if i disable interworking and just stick to the arm instruction set, code gets even bigger (of course) but it works then!
So seems to be a problem with the thumb/interworking? anyone knows how to solve this?
Have a look at this (an article on my website).
http://www.webalice.it/fede.tft/cpp_on_ … ricks.html
Using my optimized makefile and linker script the following code
#include <list>
#include "system.h"
using namespace std;
int main()
{
init();
list<int> l;
l.push_back(1);
shutdown();
}
compiles to ~13KB (all ARM, thumb would be even less).