Hello friends,
Following your instruction (tutorials/using-sparkfun-edge-board-wit … troduction), I installed all the components to build example apps that complie with Ambiq apollo3 SDK and run on SparkFun Edge board. The compilation process succeeded in 2 examples, but falied with the other ![]()
I am sending you 2 compilation logs as below. The first, built for example2, was successful. The 2nd, built for example1, was failure.
[Log for build example2]
8a3062bee638:/home/apollo3/AmbiqSuite-Rel2.0.0/boards/SparkFun_Edge_BSP/examples/example2_dual_mic_dma/gcc# make bootload
…/…/…/…/…/tools/apollo3_scripts/create_cust_image_blob.py --bin bin/example2_dual_mic_dma.bin --load-address 0xC000 --magic-num 0xCB -o bin/main_nonsecure_ota --version 0x0
Header Size = 0x80
original app_size 0x331c ( 13084 )
load_address 0xc000 ( 49152 )
app_size 0x331c ( 13084 )
w0 = 0xcb00339c
Security Value 0x10
w2 = 0x10008080
addrWord = 0xc000
versionKeyWord = 0x0
child0/feature = 0xffffffff
child1 = 0xffffffff
crc = 0x4bfc9037
Writing to file bin/main_nonsecure_ota.bin
…/…/…/…/…/tools/apollo3_scripts/create_cust_wireupdate_blob.py --load-address 0x20000 --bin bin/main_nonsecure_ota.bin -i 6 -o bin/main_nonsecure_wire --options 0x1
Header Size = 0x60
app_size 0x339c ( 13212 )
Writing to file bin/main_nonsecure_wire.bin
Image from 0x0 to 0x339c will be loaded at 0x20000
…/…/…/bsp/tools/uart_wired_update_sparkfun.py -b 921600 /dev/ttyUSB0 -r 1 -f bin/main_nonsecure_wire.bin -i 6
Connecting with Corvette over serial port /dev/ttyUSB0…
Sending Hello.
Received response for Hello
Received Status
length = 0x58
version = 0x3
Max Storage = 0x4ffa0
Status = 0x2
State = 0x7
AMInfo =
0x1
0xff2da3ff
0x55fff
0x1
0x49f40003
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
0xffffffff
Sending OTA Descriptor = 0xfe000
Sending Update Command.
number of updates needed = 1
Sending block of size 0x33fc from 0x0 to 0x33fc
Sending Data Packet of length 8180
Sending Data Packet of length 5128
Sending Reset Command.
Done.
[Log for build example1]
8a3062bee638:/home/apollo3/AmbiqSuite-Rel2.0.0/boards/SparkFun_Edge_BSP/examples/example1_edge_test/gcc# make bootload
Compiling gcc …/src/main.c
Compiling gcc …/…/…/…/…/devices/am_devices_led.c
Compiling gcc …/…/…/…/…/utils/am_util_delay.c
Compiling gcc …/…/…/…/…/utils/am_util_faultisr.c
Compiling gcc …/…/…/…/…/utils/am_util_stdio.c
Compiling gcc startup_gcc.c
Compiling gcc …/src/tf_adc/tf_adc.c
…/src/tf_adc/tf_adc.c: In function ‘am_adc_isr’:
…/src/tf_adc/tf_adc.c:62:58: warning: passing argument 2 of ‘am_hal_adc_samples_read’ makes pointer from integer without a cast [-Wint-conversion]
62 | true,
| ^~~~
| |
| int
In file included from …/…/…/…/…/mcu/apollo3/am_mcu_apollo.h:132,
from …/src/tf_adc/tf_adc.c:1:
…/…/…/…/…/mcu/apollo3/hal/am_hal_adc.h:618:53: note: expected ‘uint32_t *’ {aka ‘long unsigned int *’} but argument is of type ‘int’
618 | uint32_t *pui32InSampleBuffer,
| ~~~~~~~~^
…/src/tf_adc/tf_adc.c:64:58: warning: passing argument 4 of ‘am_hal_adc_samples_read’ from incompatible pointer type [-Wincompatible-pointer-types]
64 | &ui32NumSamples,
| ^~~~~~~~~~~~~~~
| |
| uint32_t * {aka long unsigned int *}
In file included from …/…/…/…/…/mcu/apollo3/am_mcu_apollo.h:132,
from …/src/tf_adc/tf_adc.c:1:
…/…/…/…/…/mcu/apollo3/hal/am_hal_adc.h:620:64: note: expected ‘am_hal_adc_sample_t *’ {aka ‘struct *’} but argument is of type ‘uint32_t *’ {aka ‘long unsigned int *’}
620 | am_hal_adc_sample_t *pui32OutBuffer);
| ~~~~~~~~~~^
…/src/tf_adc/tf_adc.c:61:38: error: too many arguments to function ‘am_hal_adc_samples_read’
61 | if (AM_HAL_STATUS_SUCCESS != am_hal_adc_samples_read(g_ADCHandle,
| ^~~~~~~~~~~~~~~~~~~~~~~
In file included from …/…/…/…/…/mcu/apollo3/am_mcu_apollo.h:132,
from …/src/tf_adc/tf_adc.c:1:
…/…/…/…/…/mcu/apollo3/hal/am_hal_adc.h:617:19: note: declared here
617 | extern uint32_t am_hal_adc_samples_read(void *pHandle,
| ^~~~~~~~~~~~~~~~~~~~~~~
Makefile:163: recipe for target ‘bin/tf_adc.o’ failed
make: *** [bin/tf_adc.o] Error 1
Could you take a look into?
Thanks in advance,