Using the Arduino Ethernet library with Artemis Micro Mod

In Arduino IDE 1.8.12, using board Artemis Micro Mod with the Ambiq Bootloader (Recommended). The “Sparkfun Apollo3 Boards” version is 2.0.2 in Boards Manager.

If I try to verify the Examples > Ethernet > WebClientRepeating example, I get the error below in the Arduino IDE.

If I change to Arduino Uno as the board, the program verifies fine.

Everything else with Artemis Micro Mod has been really great, and it’s been a total bummer I can’t get this to work. Any help would be greatly appreciated. Is there a way to get Ethernet working in any way on the Artemis Micro Mod? I believe my ethernet module is a Wiznet W5500 connected with SPI.

WebClientRepeating:38:1: error: 'EthernetClient' does not name a type; did you mean 'EthernetClass'?
 EthernetClient client;
 ^~~~~~~~~~~~~~
 EthernetClass
C:\Users\sdelu\AppData\Local\Temp\arduino_modified_sketch_300391\WebClientRepeating.ino: In function 'void setup()':
WebClientRepeating:49:3: error: 'Ethernet' was not declared in this scope
   Ethernet.init(5);   // MKR ETH shield
   ^~~~~~~~
WebClientRepeating:66:38: error: 'EthernetNoHardware' was not declared in this scope
     if (Ethernet.hardwareStatus() == EthernetNoHardware) {
                                      ^~~~~~~~~~~~~~~~~~
C:\Users\sdelu\AppData\Local\Temp\arduino_modified_sketch_300391\WebClientRepeating.ino:66:38: note: suggested alternative: 'EthernetClass'
     if (Ethernet.hardwareStatus() == EthernetNoHardware) {
                                      ^~~~~~~~~~~~~~~~~~
                                      EthernetClass
WebClientRepeating:72:34: error: 'LinkOFF' was not declared in this scope
     if (Ethernet.linkStatus() == LinkOFF) {
                                  ^~~~~~~
C:\Users\sdelu\AppData\Local\Temp\arduino_modified_sketch_300391\WebClientRepeating.ino: In function 'void loop()':
WebClientRepeating:91:7: error: 'client' was not declared in this scope
   if (client.available()) {
       ^~~~~~
C:\Users\sdelu\AppData\Local\Temp\arduino_modified_sketch_300391\WebClientRepeating.ino:91:7: note: suggested alternative: 'dirent'
   if (client.available()) {
       ^~~~~~
       dirent
C:\Users\sdelu\AppData\Local\Temp\arduino_modified_sketch_300391\WebClientRepeating.ino: In function 'void httpRequest()':
WebClientRepeating:108:3: error: 'client' was not declared in this scope
   client.stop();
   ^~~~~~
C:\Users\sdelu\AppData\Local\Temp\arduino_modified_sketch_300391\WebClientRepeating.ino:108:3: note: suggested alternative: 'dirent'
   client.stop();
   ^~~~~~
   dirent
exit status 1
'EthernetClient' does not name a type; did you mean 'EthernetClass'?

Here is the example’s code for reference:

/*
  Repeating Web client

 This sketch connects to a a web server and makes a request
 using a Wiznet Ethernet shield. You can use the Arduino Ethernet shield, or
 the Adafruit Ethernet shield, either one will work, as long as it's got
 a Wiznet Ethernet module on board.

 This example uses DNS, by assigning the Ethernet client with a MAC address,
 IP address, and DNS address.

 Circuit:
 * Ethernet shield attached to pins 10, 11, 12, 13

 created 19 Apr 2012
 by Tom Igoe
 modified 21 Jan 2014
 by Federico Vanzati

 http://www.arduino.cc/en/Tutorial/WebClientRepeating
 This code is in the public domain.

 */

#include <SPI.h>
#include <Ethernet.h>

// assign a MAC address for the ethernet controller.
// fill in your address here:
byte mac[] = {
  0xDE, 0xAD, 0xBE, 0xEF, 0xFE, 0xED
};
// Set the static IP address to use if the DHCP fails to assign
IPAddress ip(192, 168, 0, 177);
IPAddress myDns(192, 168, 0, 1);

// initialize the library instance:
EthernetClient client;

char server[] = "www.arduino.cc";  // also change the Host line in httpRequest()
//IPAddress server(64,131,82,241);

unsigned long lastConnectionTime = 0;           // last time you connected to the server, in milliseconds
const unsigned long postingInterval = 10*1000;  // delay between updates, in milliseconds

void setup() {
  // You can use Ethernet.init(pin) to configure the CS pin
  Ethernet.init(0);
  //Ethernet.init(10);  // Most Arduino shields
  //Ethernet.init(5);   // MKR ETH shield
  //Ethernet.init(0);   // Teensy 2.0
  //Ethernet.init(20);  // Teensy++ 2.0
  //Ethernet.init(15);  // ESP8266 with Adafruit Featherwing Ethernet
  //Ethernet.init(33);  // ESP32 with Adafruit Featherwing Ethernet

  // start serial port:
  Serial.begin(9600);
  while (!Serial) {
    ; // wait for serial port to connect. Needed for native USB port only
  }

  // start the Ethernet connection:
  Serial.println("Initialize Ethernet with DHCP:");
  if (Ethernet.begin(mac) == 0) {
    Serial.println("Failed to configure Ethernet using DHCP");
    // Check for Ethernet hardware present
    if (Ethernet.hardwareStatus() == EthernetNoHardware) {
      Serial.println("Ethernet shield was not found.  Sorry, can't run without hardware. :(");
      while (true) {
        delay(1); // do nothing, no point running without Ethernet hardware
      }
    }
    if (Ethernet.linkStatus() == LinkOFF) {
      Serial.println("Ethernet cable is not connected.");
    }
    // try to congifure using IP address instead of DHCP:
    Ethernet.begin(mac, ip, myDns);
    Serial.print("My IP address: ");
    Serial.println(Ethernet.localIP());
  } else {
    Serial.print("  DHCP assigned IP ");
    Serial.println(Ethernet.localIP());
  }
  // give the Ethernet shield a second to initialize:
  delay(1000);
}

void loop() {
  // if there's incoming data from the net connection.
  // send it out the serial port.  This is for debugging
  // purposes only:
  if (client.available()) {
    char c = client.read();
    Serial.write(c);
  }

  // if ten seconds have passed since your last connection,
  // then connect again and send data:
  if (millis() - lastConnectionTime > postingInterval) {
    httpRequest();
  }

}

// this method makes a HTTP connection to the server:
void httpRequest() {
  // close any connection before send a new request.
  // This will free the socket on the WiFi shield
  client.stop();

  // if there's a successful connection:
  if (client.connect(server, 80)) {
    Serial.println("connecting...");
    // send the HTTP GET request:
    client.println("GET /latest.txt HTTP/1.1");
    client.println("Host: www.arduino.cc");
    client.println("User-Agent: arduino-ethernet");
    client.println("Connection: close");
    client.println();

    // note the time that the connection was made:
    lastConnectionTime = millis();
  } else {
    // if you couldn't make a connection:
    Serial.println("connection failed");
  }
}

Sounds like the library might only be Uno compatible. :frowning:

Did you ever get this to work? I’m seeing the same problem with the Ethernet function board and the Artemis processor libraries. the Ethernet.h file causes a conflict.