I have some EL animated signs (very small, less than 2" square) with five EL elements. Each sign comes with six contacts: one contact for each of five elements, and a sixth, common contact.
I want to animate these signs using an Arduino and an Escudo Dos EL sequencer shield. I get that I need an external inverter (probably 3V) along with the shield. I get that I can control each of the 8 channels independently.
My question is about the common contact: can I connect one side of the eight sequencer channel outputs together to make a common connection?