Forgive me, but I am not sure this is the right place to post this, so many choices. Anyways, for over 20 years I have been using the Parallax Basic Stamp and the Propeller. I have had success using the I2C format for the HMC6352, which is no longer made. I did use that component in a satellite tracker for directv on my boat while anchored in calm waters. Yes, it worked quit well, holding to 1 degree. I have lost all the PBASIC source code for that project which includes the I2C code.
So, my question is, does anyone out there have working source code, using a BASIC STAMP for the above two items. I which to build a high temperature device for my wood burner. I just need the I2C part of the source code that would give me a temperature number using the above MCP9600 amplifier and the Type K thermocouple. I can take it from there. I have tried to read the literature on I2C, but much to complicated…
I did post this in the General Chit Chat section, but was not sure that was the right place
Thank you…