I’m a new user of the MSP430 and eZ430-F2013 boards.
I’m MAC based and will have to purchase a new PC in order to relate
to the MSP430 boards. Within a day of receiving these amazing little
MSP430 boards from TI I found that the PC world was in a new throe
of upheaval with Vista releasing and all the computer ads talking
only about that program.
I could get an older new PC with XP but the new laptops with Vista
are another step forward (at least in theory) and it would be interesting
to get one of them for this project. So I wanted to ask this forum whether
Vista worked at all with the eZ430 software yet because I’ve lived through
similar MAC changes that simply caused previous programs to quit working
altogether.
Basically I’m assuming that Vista will not work without rather extensive
upgrading of the basic eZ430 workbench program but I’m very interested
to hear from anyone on this list that has any real experience with the issue.
So far as accruing bugs with upgrades that was the same with MACs until
OSX. After that I’ve seen the effect little at all. If Vista is properly
designed it may reduce that problem too. It does suggest, however,
that the basic ‘Windows 2000’ version of the eZ430 software is not
being intensely updated to follow MS’ circuitous path up the ole’
programming mountain closely. Or that the gallons of DDT needed
to clear the bugs was excessive. TSK!
Comments from anyone?
Larry