Wav trigger - amp output

hi! i need help about how to enable the onboard amp on a wav trigger.
by default it’s disabled, i can’t modify the .ini file using the wt initmaker app because it isn’t working on my mac.
i can modify the .ini file with a text editor but i need to know what i should write in the .ini file to enable the onboard amp. there is a reference table or something?
thank you in advance.

Add the following line in the .ini file to enable the onboard mono amp:

#SPKR 1

But, if the latest Mac version 2.21 of the Configurator app (available on the Robertsonics website) isn’t working on your Mac, please describe what Mac and OS version you have and what happens when you run the app.

thank you, i fixed the ini file and now it’s working.
there is a newer version of the app? i downloaded what i found on the wav trigger page, it’s the 1.0.0
where is the newest one?
thank you!

All of the latest updates are here:

https://www.robertsonics.com/downloads

thanks!
i got the amp working.
another question, now: if i’m right, the onboard amp is rated for 2 w @ 4 ohm and 1.2 w @ 8 ohm speakers.
at 85% volume, the 5w 4 ohm speaker i got starts crackling a lot.
will it works too with two 4 ohm identical speakers in parallel, thus 2 ohm?
thanks!

I wouldn’t go any lower than 4 ohms. If that isn’t loud enough, disable the on board amplifier and use some amplified computer speakers.

thank you.