WAV Trigger playback speed/pitch control

How do I change the playback speed/pitch of the WAV Trigger? Do I need to built some circuit for this? or this is some specific connection to be done on the board?

Thanks,

PRPROG

Hi PRPROG,

To control the pitch/playback speed of a track on the WAV Trigger you’ll need to do it via the serial header/FTDI port outlined in the [Hardware Section of the WAV Trigger’s Hookup Guide. You can use the “wTrig.samplerateOffset()” function from the [Arduino Library with an Arduino. Alternatively, you can control the sample rate the via the serial header using the [Serial Control Protocol or [MIDI input with a MIDI controller.](https://robertsonics.com/wav-trigger-online-user-guide/#chapter10)](https://robertsonics.com/wav-trigger-online-user-guide/#chapter9)](GitHub - robertsonics/WAV-Trigger-Arduino-Serial-Library: WAV Trigger Serial Control Arduino Library)](https://learn.sparkfun.com/tutorials/wav-trigger-hookup-guide-v11#hardware)

Thanks TS-Mark for the quick reply.