What size drills are on the tool rack?

Would it be possible to publish a list of the drill sizes that can be used to drill holes in the pcb proto boards? Or better yet, since we are going to be dealing with plated hole sizes, a list of finished plated hole diameters would be even better.

I would feel more comfortable knowing what the available sizes are so I can set up Eagle to show the correct hole diameter information.

Thanks

look at the specs here: http://ca.goldphoenixpcb.com/, Sparky is using them and will need to meet the same requirements.

Jamie

Actually, there is no standard drill rack. You can create virtually any size aperature, no smaller than 20mil, and no larger than 750mil.

-Nathan