wh33t
November 29, 2021, 4:27pm
1
Please also suggest me a battery and an enclosure if those are also available.
Very anxious to try and replicate a product that costs us many hundreds of dollars per unit and $20/year in cloud fees.
I know battery life may not be the greatest, but that’s OK as long as the batteries are affordable or rechargeable.
Thanks so much! :mrgreen:
wh33t
November 29, 2021, 6:14pm
2
So far I’m thinking these two things plus a battery and some connectors is all I need right?
https://www.sparkfun.com/products/17381 (SparkFun Thing Plus - ESP32 WROOM (U.FL))
https://www.sparkfun.com/products/16298 (Qwiic Pressure/Humidity/Temp (PHT) Sensor - MS8607)
Can I power this all with USB power bank? Or does it need to be a LiPo pack type thing?
You’ll need an 2.4GHz antenna too but those should all work.
power bank or a lipo would be fine for power but a lipo would be more energy efficient.
wh33t
December 3, 2021, 6:54pm
4
Thank you for the reply.
How would I charge the LiPo pack once it’s dead and will I be able to have the ESP32 tell me when the battery is getting low? I presume there is some kind of script I can write to monitor battery levels?
If you read the directions, there’s a battery charger built into the ESP32 thing plus. There isn’t a way to monitor battery charge though so you’d need to build an external circuit for that or use something like the [lipo fuel gauge .](SparkFun LiPo Fuel Gauge - TOL-20680 - SparkFun Electronics )