Does anyone have a code sample that will show me how to setup my new Wifly board to connect to a wireless network using a static IP. I am using the Alpha 2 Wifly.h library to connect to my network via DHCP, but I would rather use a static IP address. I see notes in the “Readme” file for the Alpha library that give some indication that it is not supported yet. On the other hand, I see posts on the message board that indicate it can be done. Can someone set me straight? Can it be done and if so, how?
Any help or guidance would be greatly appreciated.