So after owning it for a few months I finally decided tonight to give my WiFly module a whirl, seeing as how my school has campus wide wifi (ohhh the posibilities… xD) so i hooked it up, GND-> PSGND → PC GND & 3.3 → PS 3.3 & TX to RX on RS232 & RX to TX on RS232. I opened my terminal, following the guide, and entered $$$ to enter command mode. This was what i got as following results: (In Hex because the terminal did not recognize half the chars) :
24 24 24 5F 45 91 52 D3 C9 32 42 72 7E 36 42 26 5A 46 62 3A 7E 72 5E 7A 46 0A 3E 7E 4A 42 6E 6A 0A C6 C2 C6 EA 7E E6 FA DA CE EA EE CA D6 00
First 3 Chars: 24 = $$$ to enter command mode… next several chars… not the expected CMD results…
Any and all help is greatly appreciated!
Thanks
~Matt