Sorry if this is a repeat - I just posted but can’t find it, and I need to update. I have attached the WIFLY to the Arduino UNO with the 8-pin connectors, and no lights are lit on the board. However, I used a multimeter to test voltage, and both the 3.3 and 5v are reading correctly. That said - when I load the basic code on the board, the serial monitor displays:
WiFly Shield Terminal Routine
Could not initialize bridge, locking up.
I don’t want to start haggling with the code if in fact there should be lights on the board and the problem lies with something more fundamental. Any help or suggestions would be greatly appreciated!!
Thanks,
Claudia