Hi, I just bought the module RN-131G. I managed to connect and send ascii from telnet to realterm and vice versa, But I have 2 problems.
- When trying to enter $$$ in telnet, I can access the CMD and settings, but when entered in Hyperterminal/Realterm, I get CMD then like i am typing a lot of invalid commands till I reset the board.
2. This is the most important thing: I am trying to interface analog signals to Sensor 0 - 7. I have ver 2.08 and I can not get the signals to work neither form telnet or from Realterm. I am giving it a 3.3V signal using a 22K in series with a 10K to ground (as specified in the manual). Also in the manual there is written that as of V2.06, sensor pins for reading analog signals are not supported.
Can you please tell me if anyone managed to make analog signals work? If yes can you please tell me how since I would like to avoid connecting an ADC to the 8051.
Thanks a lot