Hi everyone,
Everything works finally perfect, I succeded in connecting my Android Phone to my Arduino using a self-made TCP Server and I can transmit commands between both. My problem now is that I would like my Arduino to… “understand” what it is receiving. I mean, for example I would like to send my Arduino “up”, which would run the motors. At the moment I use SpiUartTerminal and I thought I just had to add conditions in the loop, like:
void loop() {
while(SpiSerial.available() > 0) {
Serial.print(SpiSerial.read(), BYTE);
// Here add a condition like if SpiSerial.read() == "up", handle the motor, but it can't be since the read() function return an Integer. And I think this loop isn't in the right place is it ? ^^
}
if(Serial.available()) {
SpiSerial.print(Serial.read(), BYTE);
}
Well that’s just very simple, but what I just wrote is totally wrong because SpiSerial.read() is an Int whereas up is a string, so would anyone have an idea how I could make my 2 devices understand eachother ?
Like making a big dictionnary of functions so it will be like a sinergy ^^
Maybe the TexFinder Library ? I tried to run the WebServer but it couldn’t being compiled because of this line : TextFinder finder(client); . It says there’s no matching function.
Thank you, you helped me a lot for this project and I hope I would be once able to help you back.
By the way, here’s the code I’m trying to debug:
#include "WiFly.h"
#include "Credentials.h"
#include "TextFinder.h"
Server server(80);
int instruction;
void setup() {
WiFly.begin();
if (!WiFly.join(ssid, passphrase)) {
while (1) {
// Hang on failure
}
}
Serial.begin(38400);
Serial.print("IP: ");
Serial.println(WiFly.ip());
server.begin();
}
void loop() {
Client client = server.available();
if (client) {
TextFinder finder(client); // It doesn't work here...
while (client.connected()) {
if (client.available())
{
if(Serial.available() > 0)
{
finder.find("@");
instruction = finder.getValue();
ParseInstruction(instruction);
}
}
}
// give the web browser time to receive the data
delay(100);
client.stop();
}
else
{
while(SpiSerial.available() > 0)
{
Serial.print(SpiSerial.read(), BYTE);
}
if(Serial.available())
{ // Outgoing data
SpiSerial.print(Serial.read(), BYTE);
}
}
}
void ParseInstruction(int instr)
{
switch(instr)
{
case 1:
// Here's the code
break;
case 2:
// Here's the code
break;
default:
// Here's the code
break;
}
}
However, I can’t bind my TextFinder to my client, even if I used an instruction available here: http://www.arduino.cc/playground/Code/TextFinder , so, this one:
TextFinder finder(client);
Here’s the error I get :
WiFly_WebServer:29: error: no matching function for call to ‘TextFinder::TextFinder(Client&)’
I understand the error, TextFinder parameters() are either Stream and an Integer, either a const. However, I don’t understand why it should work on the Arduino Official Website and not here…
Sorry for the double post, I got an error when I tried to edit my first message…
EDIT: I think there’s a conflict between WiFly Library’s client and Ethernet Library’s client…
I too would like to use TextFinder with the WiFly library. Did you find a solution to allow you to do so?