Hi everyone
I’m building a robot , one of its main function is to do the following :
Go to a predefined destinations.I don’t want to Use path-follower because it clashes with another main function( avoiding obstacles ) . So i figured , one way to do this , is to get several (Transmitter\Receiver) pairs with different frequency for each pair.I’ll place Transmitter1 in destination1 , Tarnsmitter2 in destination2 etc. and place all the receivers in the robot.So when Receiver1 is activated the robot will go toward Transmitter1 (destination1) and so on .
My Questions are :
can i do that using :
RF Link 2400bps Receiver - 434MHz) & RF Link Transmitter - 434MHz
and
RF Link 2400bps Receiver - 315MHz & RF Link 2400bps Receiver - 315MHz
?
can i get a third pair with different frequency ?
Thanks in advanced ![]()