Wire assemblies to go from 1 wire to 10 wires

I have a board that needs to provide 10 sets of power lines and one data line (so 10 sets of 3 wires). Now instead of getting 30 tap offs from my board as all power and grounds are the same I wanted to come from one power/ground pair off the board, then from that pair, go outside my enclosure, then split off into 10 pairs.

Obviously I can just solder a load of wires together, but I prefer not too. I was wondering are any cables sold that just fray off into multiple wires, or in-cable small junctions for 22-28AWG wire or any other pre-made component that I can just quickly use to split the wires? I will have to do 100s of these so don’t fancy hours of soldering if there is a nice quick solution?

I’d design a small PCB for that sort of thing.

Leon

What Leon said. Or just use some prototype board.

You could use multicore cable… Strip and solder all cores together at one end and splay the other end.

Thats not a bad idea, and its also easy to seal with heat shrink. Cool.