xbee - 3 module comms.

Hi all, Wonder if anyone can enlighten me.

I currently have 2 xbee 900 modules working in my hexakopter build.

One is connected to the hexa.

The other connects to an arduino and an LCD.

The hexa broadcasts a whole bunch of data and the arduino displays it (ie telemetry)

The hexa can also receive data via it’s xbee connection and i will soon have a new device (POI sender) which sends it’s own gps position twice a second (via an xbee) and the hexa can either follow it or point it’s camera to it.

Now to the question.

Can i add this third xbee to my existing pairing or will i have to switch off one of the ground side xbees while the other it running?

Ideally i’d like to still see the telemetry data while the POI sender is communicating with the hexa - as it contains lipoly level and gps fix.

ie:

xbee 1 hexa (always on)

telemetry data TO xbee 1

gps position FROM xbee 3

xbee 2

telemetry data FROM xbee 1

xbee 3

gps position TO xbee 1

All three XBees should be able to communicate as you outlined. Just ensure there is enough time for all the data to be transferred.