Xbee and arduino

Hello everyone!

I have a problem, I am a beginner and I can not find the solution …

I have one Xbee module + Arduino + Accelerometer which should send two values ​​(byte) to another Arduino + Xbee module

But I do not know how … I test something but the value received has nothing to do

Could you help me please?

Here is the code transmitter:

//Librairie
#include <LiquidCrystal.h>
//Config LCD
LiquidCrystal lcd( 12, 11, 5, 4, 3, 2) ;
//Tableau
byte tableau[2] = {0} ;

void setup(){
  Serial.begin(9600) ;
  lcd.begin(16, 2) ;
  lcd.print("Atom by STX") ;
}
void loop(){
  tableau[0] = analogRead(A0) ;
  tableau[1] = analogRead(A1) ;
  Serial.println(tableau[0]) ;                     //send values
  Serial.println(tableau[1]) ;
  lcd.setCursor(0,1) ;                              //LCD
  lcd.print("                ") ;
  lcd.setCursor(0,1) ;
  lcd.print("X= ") ;
  lcd.print(tableau[0]) ;
  lcd.setCursor(7,1) ;
  lcd.print("Y= ") ;
  lcd.print(tableau[1]) ;
  delay(750) ;
}

Here is the code recipient:

//tableau
byte tableau[2] = {0} ;

void setup()
{
  Serial.begin(9600) ;
}


void loop()
{
  if(Serial.available() > 0)
  {
    tableau[0] = Serial.read() ;
    tableau[1] = Serial.read() ;
    Serial.println(tableau[0]) ;             //i look values by IDE arduino
    Serial.println(tableau[1]) ;
    delay(750); 
  }
}