Hi guys,
I suggest this because I need it and will have to make my own probably.
I need to mod the xbee breakout like so:
Add a 4 pin .1" SIP: +5v:Gnd:Rx:Tx
Add a resistor (i am using 10k) to Rx line (for 5v signals input)(guss this should be optional)
Add optional diodes to drop from 5v to 4.2v (or 3.3v pwr regulator)
Move .1 header holes OUTBOARD of the smaller xbee holes (so we can access them from top OR bottom).
This should let me cable up a optional xbee module, and simple double tape it to the inside of my enclosure.
Thanks,
Joe.