Hi all
Whilst not new to wireless comms I am new to the whole Zigbee approach. If I could recieve some advice as to whether they are suited to my requirements I’d be grateful.
I propose to use them as an and point to a telemetry system whereby each group of XBees consists a Master back to back with a long haul radio.
The master is to broadcast over the XBee network and addressing is to be handled by the end application (Modbus) so essentially the XBees are replacing a multidrop cable network.
Each XBee network (PAN) would consist only 15 - 30 XBees, and I would prefer operate as a mesh, although likely that only a few will be out of radio range of the master, this would add redundancy and simplify configuration.
I would like to use the high power modules- 60mW.
My application involves solar power, hence low power consumption when idle is required.
I don’t entirely understand the operation of the cyclic sleep modes, ZigBee or DigiMesh, or which one would be best for my application, or indeed how the cyclic sleep works in conjunction with broadcasting.
Any help would be appreciated.
Regards
James